Apply LPCXpresso54608 for the wireless remote monitoring system of the rising temperatures

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Apply LPCXpresso54608 for the wireless remote monitoring system of the rising temperatures

1,572 Views
jackielau
Contributor I

         当前公司主要使用的是ST的F103系列的芯片,对于一般的应用来说,资源已经足够使用了。面对更复杂的应用的话,处理能力、资源方面及一些接口方面比较短缺。

         LPC546xx,上至512KFlash和200KSRAM,Cortex-M4内核,主频最高可达180MHz。从介绍资料中不难看出,LPC546xx是LPC1700系列的升级产品,拥有多达10个uart和2个CAN,还有spi、i2c、emc、sdio、lcd、enet等等接口。资源和接口是相当的可观。

         

          无线远程温升监控系统,通过传感器采集温度,将温度处理后上传给主控进行显示、存储及上传远程服务器,远程服务器进行数据的存储、显示及Web发布等。最后形成客户能够通过服务器所在局域网用户能通过浏览器访问服务器www服务,也能通过手机浏览器访问。采集终端可以采用更廉价的LPC800系统的芯片,而主控采用LPC546xx相当合适。

LPC546xx的10个串口,其中1个输出日志,其他9个负责用485总线来连接采集终端传输数据,sdio接口搭载TF卡模块,可以作为数据库,进行数据的存储,emc接口连接外部RAM进行内存扩展,lcd接口连接触摸屏进行实时数据的显示,enet接口连接3G/4G无线路由器进行数据的远程传输。也就是LPC546xx作为一个小型的数据处理、显示、传输中心。

          以前没有使用过LPC的芯片,不过前段时间参加NXP社区的兑换活动,兑换了一块LPC824breakout开发板,进行了芯片的简单学习。在学习过程中,对LPC芯片灵活的开关矩阵映像深刻。故想申请此款开发板来设计无线远程温升监控系统的产品原型。

Labels (1)
0 Kudos
Reply
0 Replies