Apply LPCXpresso54608 for Vehicle positioning system based on image recognition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Apply LPCXpresso54608 for Vehicle positioning system based on image recognition

773 次查看
jianghaoyu
Contributor I

I'm in the development of vehicle positioning system based on image recognition, within a certain space principle is through the multiple video signal to collect the captured image signal, through optical flow, distance analysis processing, fusion positioning the objects being measured the three-dimensional coordinates of points in space, and calculate the movement direction, speed and acceleration of the object, upload the first machine. Project image algorithm part and upper machine part has been completed, but high performance processors are needed as carrying platform, therefore, I apply for this activity's LPCXpresso54608 development board.

I hope LPCXpresso54608, such a high-performance processor with Cortex-M4 kernel of can do perfect in my design,and thanks to NXP community.

标签 (3)
标记 (1)
0 项奖励
回复
0 回复数