ADC on LPC1788

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC on LPC1788

1,009 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by williamjsell on Mon Dec 30 16:52:14 MST 2013
I am trying to get some signs of life out of the ADC.  I have this init seqeunce, but I just get either 0x0000FFF or 0.  Am i missing something here?  If I run this code init on my embedded artists board (albeit one channel only), the ADC works fine.  On my custom board there is no sign of life.  Any ideas?

void Init_LPC_ADC(void)
{

    //init the ADC to the 400K samples per second
    ADC_Init(LPC_ADC, 400000);
//set the function up for the pin
    PINSEL_ConfigPin (0, 12, 3); //ADC0 channel 6
    PINSEL_ConfigPin (0, 13, 3); //ADC0 channel 7
    PINSEL_ConfigPin (0, 23, 1); //ADC0 channel 0
    PINSEL_ConfigPin (0, 24, 1); //ADC0 channel 1
    PINSEL_ConfigPin (0, 26, 1); //ADC0 channel 3
    PINSEL_ConfigPin (1, 31, 3); //ADC0 channel 5
//disable the digital pin mode on the chip
    PINSEL_SetAnalogPinMode (0, 12, ENABLE);
PINSEL_SetAnalogPinMode (0, 13, ENABLE);
PINSEL_SetAnalogPinMode (0, 23, ENABLE);
    PINSEL_SetAnalogPinMode (0, 24, ENABLE);
    PINSEL_SetAnalogPinMode (0, 26, ENABLE);
PINSEL_SetAnalogPinMode (1, 31, ENABLE);
//disable the interrupts on the channel
    ADC_IntConfig(LPC_ADC, MHI, DISABLE);
    ADC_IntConfig(LPC_ADC, MLO, DISABLE);
    ADC_IntConfig(LPC_ADC, RTD, DISABLE);
    ADC_IntConfig(LPC_ADC, BDTEMP, DISABLE);
    ADC_IntConfig(LPC_ADC, PWR1, DISABLE);
    ADC_IntConfig(LPC_ADC, PWR2, DISABLE);   
//set the channel to enable
ADC_ChannelCmd(LPC_ADC, MHI, ENABLE); 
ADC_ChannelCmd(LPC_ADC, MLO, ENABLE);
    ADC_ChannelCmd(LPC_ADC, RTD, ENABLE);
    ADC_ChannelCmd(LPC_ADC, BDTEMP, ENABLE);
    ADC_ChannelCmd(LPC_ADC, PWR1, ENABLE);
    ADC_ChannelCmd(LPC_ADC, PWR2, ENABLE);
//set to burst mode
ADC_BurstCmd(LPC_ADC, SET);
}
标签 (1)
0 项奖励
回复
1 回复

891 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Sat Jan 25 11:09:37 MST 2014
Hi William,
Did you use burst mode with EA development board as well?
Notice there is a burst mode related errata item related with this part. Please check it out.
Regards!
0 项奖励
回复