ADC bits of LPC4370FET256 and LPC4370FET100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC bits of LPC4370FET256 and LPC4370FET100

ソリューションへジャンプ
1,318件の閲覧回数
diverger
Contributor II

In the part selector in LPC4300 Series: High-Performance Microcontrollers (MCUs) based on Arm® Cortex®-M4/M0 Cores|NXP , I find in the 'ADC(bits)' column, LPC4370FET100 shows 12, and LPC4370FET256 shows 10. But I can't find any other special description of this in the their datasheet. Is it just a 'typo', or this ADC bits of FET256 is really can only achieve 10bits?

1.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,226件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hua,

     No, the web selection is not correct, LPC4370FET256 can support both 10 bit ADC(ADC0,1) and 12bit ADC, but LPC4370FET100 just can support 12-bit ADC, it doesn't have the 10 bit ADC.

   You can find this information in the LPC43xx user manual:

https://www.nxp.com/docs/en/user-guide/UM10503.pdf 

pastedImage_2.png

pastedImage_3.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,227件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hua,

     No, the web selection is not correct, LPC4370FET256 can support both 10 bit ADC(ADC0,1) and 12bit ADC, but LPC4370FET100 just can support 12-bit ADC, it doesn't have the 10 bit ADC.

   You can find this information in the LPC43xx user manual:

https://www.nxp.com/docs/en/user-guide/UM10503.pdf 

pastedImage_2.png

pastedImage_3.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,226件の閲覧回数
diverger
Contributor II

Thanks for your answer

0 件の賞賛
返信