ADC VREFN in LPC5514JBD64E

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ADC VREFN in LPC5514JBD64E

跳至解决方案
949 次查看
embedded_eng_
Contributor III

Hi,

I'm planning a PCB with the LPC5514JBD64E MCU.

The user manual specify that "VREFL is always from an external pin and must be at the same voltage potential as VSSA"  (39.4.1)

UM11295, https://www.mouser.com/pdfDocs/UM11295.pdf

 

 

On the other hand, the datasheet specify that VREFN is not connected to an external pin(64 pin HTQFP) (Table 3. Pin description)

https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf

 

How can I use the ADC?

Does VREFN is internally connected to GND?

 

 

 

0 项奖励
回复
1 解答
935 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  embedded_eng_

After confirm with internal,  VREFN is tied to VSSA internally.

 

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
1 回复
936 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  embedded_eng_

After confirm with internal,  VREFN is tied to VSSA internally.

 

 

BR

Alice

0 项奖励
回复