• ACSafe10.axf: Error: L6220E: Load region LR_IROM1 size (57352 bytes) exceeds limit (57344 bytes). Region contains 34 bytes of padding and 248 bytes of veneers (total 282 bytes of linker generated content).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

• ACSafe10.axf: Error: L6220E: Load region LR_IROM1 size (57352 bytes) exceeds limit (57344 bytes). Region contains 34 bytes of padding and 248 bytes of veneers (total 282 bytes of linker generated content).

3,127件の閲覧回数
steve_young1
Contributor I

All,

I just starting getting this linker error when adding new code to an existing LPC2132FBD64/01 project.  I believe it means there is no more code space available, is this correct?

I am using Keil ARM Basic 4.1 and the target options are set as RO Memory area IROM1: 0x2000 len 0xE000.  Are these values correct for allotting all available code space?

Any suggestions for squeezing a bit more into this processor?

Thanks in advance.

0 件の賞賛
返信
0 返答(返信)