12 VDC motor speed and direction control using GPIO and Timer interrupt using current sensor with LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

12 VDC motor speed and direction control using GPIO and Timer interrupt using current sensor with LPC1768

620 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravindra on Mon Apr 27 11:03:19 MST 2015
Hello Together,

I have uploaded few files related to 12VDC motor control. create the project and build to get the hex file. Bin file is not generated.

I have used the LPC1768 board from NGX technoloigies for code validation.

Thanks
Ravindra

Original Attachment has been moved to: src.rar

标签 (1)
0 项奖励
回复
0 回复数