请帮我看看LPC1769下载电路有问题吗,下不了程序

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

请帮我看看LPC1769下载电路有问题吗,下不了程序

1,251件の閲覧回数
wujiaqiang
Contributor I

请帮我看看LPC1769下载电路有问题吗,下不了程序

156218_156218.png20160722100923.png

156219_156219.png20160722101117.png

156220_156220.png20160722101215.png

ラベル(2)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,025件の閲覧回数
wujiaqiang
Contributor I

After many days,I think I find the answer,the lpc1769 need 10 needle LPC - link 2 downloader to download the program

0 件の賞賛
返信

1,025件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

After had a brief a look through the sch above, I didn't find any apparent problems with it except the R1, it have to be removed.

So I'd highly recommend you to refer to the attachment for details.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信