請問我要用LPC1518JBD64 這個MCU做開發 是要使用怎麼的開發環境

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

請問我要用LPC1518JBD64 這個MCU做開發 是要使用怎麼的開發環境

831 Views
frank_hsu
Contributor I

Dear 先進

由於之前都是用STM系列M0的MCU搭配Keil(因為是M0所以用Keil 不用錢)做開發,現在想改用這一個 LPC1518JBD64(M3),這樣就無法用Keil這個開發環境,不知道NXP的開發環境軟體是什麼 ,是要裝

MCUXpresso 這個軟體來開發嗎

多謝

Labels (1)
0 Kudos
Reply
1 Reply

656 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello frank hsu,

Yes, MCUXpresso IDE is our newest IDE, it supports LPC1518 and it's completely free.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply