申请LPC54608开发板

cancel
Showing results for 
Search instead for 
Did you mean: 

申请LPC54608开发板

195 Views
thoomanwang
Contributor IV

当前我公司正在开发一款产品,基于LPC1114和LPC4076两款MCU,当前产品已经完成原型开发,正在进行产品的基本功能测试工作。

经过查看LPC54608的技术资料,感觉LPC54608比较适合我们2017年另外一款产品的设计,希望能够进行测试一下,以确定LPC54608的性能。

在LPC基于M4内核的MCU中,最大的感觉就是没有小封装的,基本上管脚都在100个以上,但是在有些应用中主要使用基于M4内核MCU的高性能及浮点运算功能,但是外接器件很少(基本上有1~2uart、1~2个SPI、1~2个IIC,再有不超过20个其他的接口及IO口即可满足需要),而且板子空间受限制,这时因为所有的基于M4系列内核的LPC系列MCU就无法选择了。

当然了,NXP公司还有K系列MCU部分能满足需要例如K02,但是经过测试发现K02 MCU还是存在一些问题,少PIN的MCU当前Atmel、Infineon、ST都有相关产品,强烈希望NXP也能退出类似的产品。

0 Kudos
1 Reply

67 Views
thoomanwang
Contributor IV

已接收到审核通过的邮件,请问怎样领取

LPC54608开发板?

0 Kudos