求助:LPC4350的SPIFI接口无法访问N25Q256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

求助:LPC4350的SPIFI接口无法访问N25Q256

1,073 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dpliu on Tue Jan 22 22:12:55 CST 2013
使用SPIFI的例程,init函数可以执行,obj结构体有更新,但是erase和program函数都不能执行,
返回错误代码是0x200003,指示超时。请问这是什么原因?
Labels (1)
0 Kudos
Reply
7 Replies

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wwllzz on Tue Feb 04 22:59:49 CST 2014
你这问题有一年了 不知现在进展如何 我是使用SPIFI_DRV_m0.LIB 烧写是用M4干的 工具是TKscope的AK100Pro 没有烧写报错. 在M0运行时 spifi_init(&obj, CSHIGH, S_RCVCLK | S_FULLCLK, SPIFI_MHZ) 返回0 就是说正常了 可真正存取0x14000000地址时发现是0xffffffff, 还有查看变量0bj.base居然是0x80000000, 难道是初始化后自动采用0x80000000地址范围不可调试?
0 Kudos
Reply

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jason168 on Mon May 27 05:34:13 CDT 2013

NXP LPC43xx谈论群  208457913

0 Kudos
Reply

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jason168 on Mon May 27 05:34:07 CDT 2013

NXP LPC43xx谈论群  208457913

0 Kudos
Reply

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jason168 on Mon May 27 05:34:03 CDT 2013

NXP LPC43xx谈论群  208457913

0 Kudos
Reply

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jason168 on Mon May 27 05:33:59 CDT 2013

NXP LPC43xx谈论群  208457913

0 Kudos
Reply

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jason168 on Mon May 27 05:33:57 CDT 2013

NXP LPC43xx谈论群  208457913

0 Kudos
Reply

1,057 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alan_nn on Mon Feb 18 20:21:36 CST 2013
一般可能还是初始化并没有成功。没碰过此问题,具体原因得调试了,建议可将SPIFI的时钟试试不同的频率看看
0 Kudos
Reply