LPCXpresso54608: Getting Started with KEIL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso54608: Getting Started with KEIL

LPCXpresso54608: Getting Started with KEIL

Now that you've downloaded & unzipped your LPCXpresso54608 SDK, let's open KEIL uVision IDE.

Note: you must have at least uVision version 5.22.0.0 to use this board

Before we start utilizing uVision we must make sure that we have the relevant packs installed to work with the LPCXpresso54608 board.

Select the Pack Installer on the toolbar.

pastedImage_1.png

The Pack installer shows you which parts and boards for which you have support.

pastedImage_3.png

On the left hand side you see a variety of different manufacturers. The easiest way to search will be to type 'lpc' into the search right below the devices tab. Then select 'LPC54000 Series'.

pastedImage_4.png

On the right hand side under the packs tab you will see one item listed under 'Device Specific' called 'Keil::LPC54000_DFP' click on install

Note: Version 2.1.0 released on 10-18-2016 added LPC5460x support. If you had downloaded this pack before go to Packs>Check for Updates at the top to download the latest version

pastedImage_6.png

Once installed the diamond will turn green. To double check we are ready, select boards on the left side and search  'lpcxpresso54'. You will notice that our board is green indicating we have support for it in uVision.

pastedImage_7.png

Now we can close the Pack Installer to return to uVision

Select File>Open and navigate to the location you unzipped your SDK download.  By the way, within this folder there are plenty of SDK based demos for you to explore our microcontroller.  We will use one of them to guide you through this tutorial, but definitely take time to try all of them!

Navigate to boards>lpcxpresso54608>demo_apps>touch_cursor>mdk, change file type to ''Project Files (*.uvproj, *.uvprojx) and select 'touch_cursor'

pastedImage_1.png

Once opened, select 'Build' right above the Project window.

pastedImage_2.png

Once the Build Output window tells you that you have successfully built the program select the 'Start/Stop Debug Session' icon.

pastedImage_3.png

Note: You may receive a warning if you have a size limitation on the license you are using. If you do get a warning you can resolve licensing issues by going to File>License Management.

Once the debug session has been started select 'Run' on the left side

pastedImage_5.png

Once you have successfully flashed the board with this demo you will see the following,

pastedImage_12.png

This demo utilizes the touch interface on the screen to read where you are touching and updates the cursor position to the last known location.

 

Remember that other demos and sample code are provided in the root folder of the SDK download.  

Be sure to explore these demos and reach out on the community if you need help!

ラベル(2)
コメント

One thing I had to do was to remove JP5. It was installed at delivery (manual says it is open by default) and Keil would not see the DAP. Once JP5 was removed, all worked :smileyhappy:

Udklip.PNG

Important note!    The boards don't necessarily come with the CMSIS-DSP debugger.    Mine came with the J-Link firmware.    The project settings need to be changed to use the J-LINK.   Also,  the SDK projects don't have the "Download to flash and Verify" check boxes set in the "Download options" when using the Keil tools.

pastedImage_1.png

評価なし
バージョン履歴
最終更新日:
‎12-19-2016 04:07 PM
更新者: