LPC55Sxx SB2 loader vulnerability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55Sxx SB2 loader vulnerability

LPC55Sxx SB2 loader vulnerability

A vulnerability (CVE-2022-22819) has been identified on select NXP processors by which a malformed SB2 file header sent to the device as part of an update or recovery boot can be used to create a buffer overflow. The buffer overflow can then be used to launch various exploits.

Refer to the attached bulletin for more information.

 

09/26/2022 - Bulletin updated to include fix datecode information.

11/01/2022 - Bulletin updated with clarification that mixed datecodes are RT600 only.

 

 

附件
100% 有帮助 (1/1)
版本历史
最后更新:
‎11-01-2022 12:55 PM
更新人: