Where can I find more information regarding the LPC175x/6x Flash erase/program time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find more information regarding the LPC175x/6x Flash erase/program time?

1,161 Views
lpcware-support
Senior Contributor I

The erase time is 100±5% ms. This is independent of processor clock speed. You can erase one sector in 100 ms, or you can erase multiple sectors in the same time. Hence, a complete chip erase can be done in 100ms.

Programming time is 1.0±5% ms per Flash page (256 bytes). The programming time is given for writing 256 bytes from RAM to the flash. Data must be written to the flash in blocks of 256 bytes.

0 Kudos
Reply
0 Replies