What is the sample point for?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the sample point for?

19,333 次查看
lpcware
NXP Employee
NXP Employee

The sample point is the location, typically given as a percent value, inside each bit period where the CAN controller looks at the state of the bus and determines if it is a logic zero (dominant) or logic one (recessive). All CAN controllers allow this point to be configured and it is always specified as a percentage from the start of the bit period.
The location of the sample point is a trade-off. An early sample point decreases the sensitivity to oscillator tolerances and allows lower-quality oscillators. A late sample point allows for a longer signal propagation time and therefore a longer bus. A later sample point is useful for non-ideal bus topologies.
The CAN-in-Automation user’s group makes recommendations of where the sample point should be for various bit rates, with 87.5% the most common.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数