What is the required accuracy for the regulator input to the LPC17xx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the required accuracy for the regulator input to the LPC17xx?

1,741 次查看
lpcware-support
Senior Contributor I

The internal voltage regulator voltage will always regulate around 1.8V where the external input voltage can range from 2.4V to 3.6V over the temperature range of -40C to 85C.

标签 (2)
标记 (2)
0 项奖励
回复
0 回复数