What is the importance of the internal regulators on LPC176x? Specifically, what is the accuracy of the internal regulators?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the importance of the internal regulators on LPC176x? Specifically, what is the accuracy of the internal regulators?

1,890 Views
lpcware-support
Senior Contributor I

The internal voltage regulator will convert the external 3.3V to 1.8V. The 1.8V regulator powers the core domain, PLL, main oscillator, IRC with low power consumption.

As a result, the device is single supply device since the IOs supply shares the same range as the regulator supply input.

Labels (2)
Tags (2)
0 Kudos
Reply
0 Replies