The CAN controller goes into bus off mode when my application tries to send a CAN message. There is no activity on the CAN bus. Why?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The CAN controller goes into bus off mode when my application tries to send a CAN message. There is no activity on the CAN bus. Why?

4,277件の閲覧回数
lpcware
NXP Employee
NXP Employee

There are many causes of this and all relate to an issue between the CAN controller and the bus. For example no CAN transceiver, CAN transceiver disabled, broken connection between the CAN_L/H pins and the CAN controller.

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

ラベル(1)
  • CAN

タグ(1)
0 件の賞賛
返信
0 返答(返信)