I need BSDL files for 176x / 175x. Where can I find one?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need BSDL files for 176x / 175x. Where can I find one?

815 Views
lpcware-support
Senior Contributor I

Boundary scan is not implemented on 176x/175x, therefore, there is no BSDL file available.

To check the MCU pin connection of the board, it is recommended that the user create their own software, to read the input pins, and to write HIGH / LOW to the output pins. Then the data can be dumped into serial port (or any available output peripheral or stored in the internal SRAM then read by JTAG).

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies