Does the LPC17xx family of microcontrollers comply with IEC60335 safety standards?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the LPC17xx family of microcontrollers comply with IEC60335 safety standards?

1,048件の閲覧回数
lpcware-support
Senior Contributor I

Yes, NXP has developed an IEC60335 library that can be used with any of our Cortex-M3 based microcontrollers. Application note AN10918 has been written as a guide to use and implement the library. The application note can be downloaded from http://www.nxp.com/documents/application_note/AN10918.zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)