Can I wake up the part on CAN bus activity?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I wake up the part on CAN bus activity?

5,076件の閲覧回数
lpcware
NXP Employee
NXP Employee

This depends on the microcontroller used and what wakeup sources it allows.
LPC1800/4300: the event router allows wakeup via CAN from sleep mode. It allows wakeup from other power modes through the wakeup pins therefore an idea is to connect CAN_RX to a wakeup pin.
LPC11C00: the WAKEUP pin could be connected to CAN_RX. Note that the part can only go into deep sleep mode if there is no activity on the CAN bus first (which would mean the WAKEUP pin is high).

"FAQ contribution from Embedded Systems Academy, experts in CAN bus. For more information visit www.esacademy.com"

ラベル(1)
  • CAN

タグ(1)
0 件の賞賛
返信
0 返答(返信)