Are there Ethernet bootloaders available for LPC1700 and LPC2300/2400? If so, where can I find it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there Ethernet bootloaders available for LPC1700 and LPC2300/2400? If so, where can I find it?

1,376 Views
lpcware-support
Senior Contributor I

Ethernet bootloaders are available as part of the Flash Magic tool ( www.flashmagictool.com). After installing Flash Magic, you can find the bootloader in the Flash Magic\Ethernet Bootloader directory (C:\Program Files (x86)\Flash Magic\Ethernet Bootloader in a Windows x64 environment). An application note is available for download from www.nxp.com/documents/software/AN10744_Ethernet_Bootloader.zip

Labels (3)
0 Kudos
Reply
0 Replies