the MSD_CDC example cannot find SD_esdhc_kinetis.h and neither can I

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the MSD_CDC example cannot find SD_esdhc_kinetis.h and neither can I

ソリューションへジャンプ
1,123件の閲覧回数
r2djoe
Contributor I

<gently grumbles> this example is very unusable, what with the having to not copy it out of the examples folder (the copy-projects thing is forbidden because of the way the project is set up) and having to hack windows to accept the usb driver (I totally accept that NXP/Freescale shouldn't have to certify their demo device driver but it's still a hack to ask devs to reboot and mess around in boot settings) and now this file is missing. Oh and also I already had to figure out and pull in a bunch of other dependencies which are undocumented and in obscure places.

 

AND ALSO: I've filled in the 'ask this question' about 5 times now, and it keeps redirecting me to different parts of NXP/Freescale's sites asking me to log in and then subsequently loses the question ....

 

ANYWAY, if anyone has any idea where I can find this file (which is required when moving the dev_msd_cdc_bm_twrk60d100m project between RAM_DISK_APP and SD_CARD_APP modes that would be great.

ラベル(1)
1 解決策
864件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joe,

We have provided a solution for this issue, please kindly refer to How to add SD card support in the composite msd_cdc demo[KSDK 1.3] for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
865件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joe,

We have provided a solution for this issue, please kindly refer to How to add SD card support in the composite msd_cdc demo[KSDK 1.3] for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------