I noticed when I first tried out a few of the KSDK examples that the terminal emulator running on the host PC had to have the correct baud rate set up to match the FRDM board, despite communicating over USB. I was surprised by this and thought that the terminal emulator baud rate would have been irrelevant.
Can anyone explain why this is the case? I am using the Segger J-Link Firmware for OpenSDA on the FRDMK64.
已解决! 转到解答。
Hi,
Regarding the baudrate of virtual COM with USB, based on protocol of the USB virtual COM class, the virtual COM has "control interface" and "data interfcae", when you change the baudrate in the tools such as hyperterminal run in host side, the host will send the new baudrate to device via "control interface" of USB, this is a dynamic process.
Hope it can help you.
BR
Xiangjun Rong
Hi,
Regarding the baudrate of virtual COM with USB, based on protocol of the USB virtual COM class, the virtual COM has "control interface" and "data interfcae", when you change the baudrate in the tools such as hyperterminal run in host side, the host will send the new baudrate to device via "control interface" of USB, this is a dynamic process.
Hope it can help you.
BR
Xiangjun Rong