porting the lwip_ping_demo from K 60D10 to K61FN1M0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

porting the lwip_ping_demo from K 60D10 to K61FN1M0

1,190 次查看
jackyzeng
Contributor I

I am trying to port the lwip_ping_demo from K 60D10 to K61FN1M0.Which files I need to modify in lwip project and ksdk_platform_lib?  Any suggestions about this porting. Thank you very much!

标签 (1)
2 回复数

1,005 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Jacky,

K60D10 is Kinetis 100MHz part, while K61FN1M0 is Kinetis 120MHz part, so maybe you can refer to http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4526.pdf  before you start the porting.

Hope that helps,


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,005 次查看
jackyzeng
Contributor I

Thanks for your help.

0 项奖励
回复