is there some example using freemaster+frdm-k64f + PE+kds3.0+ sdk 1.2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is there some example using freemaster+frdm-k64f + PE+kds3.0+ sdk 1.2?

Jump to solution
3,785 Views
jordangarcia
Contributor II

Hey guys, I'm an engineering student and I´d like to use freemaster componet in the new kds and sdk versions (3.0 and 1.2)  to watch my global variables (like codewarrior does) and watch them in a graphic mode.

 

Could you provide me an example using frdm-k64+pe+sdk ? Please

 

Thanks.

Labels (1)
1 Solution
3,097 Views
BlackNight
NXP Employee
NXP Employee

Hi Jordan,

attached is an example I'm using in one of my courses.

I plan to write a tutorial about it,but have not finished it yet.

I hope this helps,

Erich

View solution in original post

4 Replies
3,098 Views
BlackNight
NXP Employee
NXP Employee

Hi Jordan,

attached is an example I'm using in one of my courses.

I plan to write a tutorial about it,but have not finished it yet.

I hope this helps,

Erich

3,096 Views
BlackNight
NXP Employee
NXP Employee

Attached is a hands-on slide deck for a hands-on workshop which shows using Kinetis Design Studio v3.0.0, Kinetis SDK v1.2, FreeMASTER v1.4 with the FRDM-K64F board.

I hope this this is useful.

Erich

3,096 Views
rogerchaplin
Contributor II

This slide deck is excellent. Your instructions are very clear, and I was able to use them to get FreeMASTER up and running on a TWR-KV31F512 board even though you wrote the tutorial for a different board. Well done!

0 Kudos
Reply
3,096 Views
jordangarcia
Contributor II

Thanks Erich :

The information is great (like always) and the example too. :smileywink:

Regards.

Jordan.

0 Kudos
Reply