has anybody tried PWM examples in KSDK2.0 for k64F?If so, any application notes?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

has anybody tried PWM examples in KSDK2.0 for k64F?If so, any application notes?

1,478 Views
girishkumarch
Contributor II

Not able to find example applications related to PWM ysing FlexTimer APIs.Has anybody tried using PWM in KSDK 2.0 & KDS 3.0. !

Labels (1)
4 Replies

1,356 Views
girishkumarch
Contributor II

Thank you,David. will check the same today.

0 Kudos
Reply

1,356 Views
DavidS
NXP Employee
NXP Employee

Iva's notes probably will be more helpful but I do have a project you can review and test on FRDM-K64F attached.

Note/comments in the main.c.  Look for "//DES".

Unzip to following folder:

C:\NXP\KSDK_v2\SDK_2.0_FRDM-K64F_KDS\boards\frdmk64f\user_apps

Regards,

David

1,356 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Girish,

I will prepare such example for you.

Best Regards,

Iva

0 Kudos
Reply

1,356 Views
girishkumarch
Contributor II

Thank you Iva,

0 Kudos
Reply