baud rate 19200 achieved with settings at 16500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

baud rate 19200 achieved with settings at 16500

1,713 Views
andrewmeyerbti
Contributor III

KDS V2.0.0,

  KSDK 1.1.0 Eclipse Update1.0.0.b141204com.freescale.processorexpert.ksdk-1.1.0.sp.feature.groupFreescale Semiconductor
  Processor Expert for KDS2.0.0.RT6_b1444-1070com.freescale.processorexpert.feature.kds.feature.groupFreescale Semiconductor

 

After some effort I was able to get an ASyncroSerial component to work on my FRDM-KE04Z board by adjusting the component baud rate to 16500 and leaving hyperterminal set at 19200.  Living with it for now.

Labels (1)
2 Replies

1,276 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Andrew:

In addition to help provided by Mark, keep an eye to the internal oscillator frequency. There seems to be a bug not fixed in Processor Expert, which lists by default an Internal Oscillator clock of 32.768 kHz:

KE_clock.png

The correct trimmed value out of the factory should be 37.5 kHz as stated in the datasheet:

KE_factory_trim.png

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,275 Views
mjbcswitzerland
Specialist V

Andrew

I have attached a binary for the FRDM-KE04Z as reference which has output on the UART (virtual COM UART 0) at 19200Baud. You can check it as comparison and look at registers with the debugger if needed. I don't use PE or KDS but the settings were made as for any other processor part.

To check are:

1. The PLL runs at 40MHz and the bus clock at 20MHz

2. UART0 is derived from the bus clock and so needs a divide value of 65 (0x41), resulting in a Baud rate of 19'230 (16x oversampling clock)

Check the values that you have from the generated settings to see whether there is an error or whether you maybe set a clock up differently to expected.

Regards

Mark

http://www.utasker.com/kinetis.html

0 Kudos
Reply