Why cant i change CAN bus bit rate to 500kbps on MK20?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why cant i change CAN bus bit rate to 500kbps on MK20?

1,403件の閲覧回数
yarannan
Contributor III

Hi there,

I am using KSDK1.2 on KDS 3.0 with MK20DX256VL10.

I tried to follow the K60 CAN example. And so far, two

of can bit rate configuration (125kbps and 250 kbps) works.

Once i move up to 500kbps. It doesnt work anymore.

The physical interface I used is NXP TJA1051. It could go

up to 2Mbits/s.

 

Is there any thing that I probably missed from above?

Please point out. I am really frustrated...

 

Thanks,

 

Yaran

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,027件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer below FlexCAN bit timing setting for 500KHz, which is based on TWR-K60D100M with bus clock 48MHz:

2015-12-11_14-58-01.png

Wish it helps.
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信