Hi there,
I am using KSDK1.2 on KDS 3.0 with MK20DX256VL10.
I tried to follow the K60 CAN example. And so far, two
of can bit rate configuration (125kbps and 250 kbps) works.
Once i move up to 500kbps. It doesnt work anymore.
The physical interface I used is NXP TJA1051. It could go
up to 2Mbits/s.
Is there any thing that I probably missed from above?
Please point out. I am really frustrated...
Thanks,
Yaran
 
					
				
		
 Hui_Ma
		
			Hui_Ma
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Please refer below FlexCAN bit timing setting for 500KHz, which is based on TWR-K60D100M with bus clock 48MHz:
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------