Where can I find the KSDK for KE06Z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find the KSDK for KE06Z?

1,512 Views
steeevo
Contributor II

I'm looking to work with the KSDK on th Freedom KE06Z but the board doesn't seem to be found in any KSDK downloads or available for build by the Kinetis Expert online tool.
Any help would be appreciated.

 

Thank you

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

1,307 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Steven.

Unfortunately there is no plan to support neither Kinetis E nor Kinetis EA in SDK.

Kinetis E are 5V /Robust and the peripherals are different and this is the reason why it´s not supported.

Have a great day!

Best Regards,

Iva

0 Kudos
Reply

1,307 Views
justin124
Contributor I

Hi Iva,

     I'm a newer for Kinetis MCU, and the KE06 series are my first met. I want know if I use KDS 3, which SDK should I install for KE06? Thank you!

Regards!

Justin

0 Kudos
Reply

1,307 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Lijie,

KSDK does not support any of KE/KEA family because they are 5V and the peripherals are different.

The best choice is to use KDS 3 with PEx and use LDD components to initialize and configure their peripherals.

Best Regards,

Iva

0 Kudos
Reply