Upgrade from KSDK 1.2.0 to KSDK 1.3.0, problem with fsl_mpu

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Upgrade from KSDK 1.2.0 to KSDK 1.3.0, problem with fsl_mpu

1,745 次查看
jesperpape
Contributor II

Hello,

 

I have a project for the TWR-K65F180M board. After upgrading the project from KSDK 1.2.0 to 1.3.0 I am getting an error on the fsl_mpu component:

 

89702_89702.pngpastedImage_1.png

 

89455_89455.pngpastedImage_0.png

 

Any help on solving this?

标签 (1)
0 项奖励
回复
4 回复数

1,555 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  ,

Could you please send you project to me , i will check it on my side .

And i create one new simple project on my side , KDS3.0 + SDK1.3, after add the component of "fsl_mpu" , there is no error :

pastedImage_0.png

BR

Alice

0 项奖励
回复

1,555 次查看
jesperpape
Contributor II

Yes, I can create a new project also without problems. The problem is upgrading from KSDK 1.2.0 to 1.3.0. The problem can be easily recreated by creating a new project using KDSK 1.2.0 and then upgrading it to KDSK 1.3.0. I use MQX standard configuration in the osa1 component. I'm attaching the small KDS project where the problem is recreated - before and after upgrading.

BR

Jesper

0 项奖励
回复

1,555 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jesper,

Sorry for that the KSDK1.2 project can not porting to KSDK1.3 , they are much different , only can create a new project .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,555 次查看
jesperpape
Contributor II

Hello Alice,

Not so great...

But I found out it is possible to upgrade the project by temporarily setting the OS to "Bare Metal" in the osa component. After the upgrade I set it back to "MQX".

BR

Jesper

0 项奖励
回复