[Solved] FRDM-K64F -> SDK_2.6.0 -> lwip_mqtt(bare metal)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Solved] FRDM-K64F -> SDK_2.6.0 -> lwip_mqtt(bare metal)

1,753 Views
yorktsai
Contributor I

Hello,
I am looking for a lwip_mqtt (bare metal) example, I want to use it to do some applications,

but currently in the FRDM-K64F SDK_2.6.0, lwip_mqtt example only provides FreeRTOS version.
I would like to ask if there are examples of lwip_mqtt (bare metal) or other suggestions can be provided for my reference, thank you!

0 Kudos
Reply
2 Replies

1,564 Views
danielchen
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,564 Views
yorktsai
Contributor I

Hi Daniel,

The part of the bare metal, I have already made it, the reference link and example are the same as you.
Thank you for your reply.:smileylaugh:

Regards

York

0 Kudos
Reply