Hi,
I am using a Kinetis KM34Z128AXXX5 to write SPI data over DMA. The SPI and DMA have been setup correctly as far as my understanding goes, but there is no data on the SPI lines when I check with an oscilloscope. The SPI and DMA code is as below:
SE_INT08U data[4] = { 0xAA,0xAA,0xAA,0xAA };
#define SPI_MODULE_CUSTOM_CONFIG \
(tSPI){ \
/* C1 */ CLR(SPI_C1_SPIE_MASK)|SET(SPI_C1_SPE_MASK)|CLR(SPI_C1_SPTIE_MASK)| \
/* .. */ SET(SPI_C1_MSTR_MASK)|CLR(SPI_C1_CPOL_MASK)|CLR(SPI_C1_CPHA_MASK)| \
/* .. */ CLR(SPI_C1_SSOE_MASK)|CLR(SPI_C1_LSBFE_MASK), \
/* C2 */ CLR(SPI_C2_SPMIE_MASK)|CLR(SPI_C2_SPIMODE_MASK)| \
/* .. */ SET(SPI_C2_TXDMAE_MASK)|CLR(SPI_C2_MODFEN_MASK)| \
/* .. */ CLR(SPI_C2_RXDMAE_MASK)|CLR(SPI_C2_SPISWAI_MASK)| \
/* .. */ CLR(SPI_C2_SPC0_MASK), \
/* C3 */ 0, /* C3 is not used for SPI0 module due to no FIFO support */ \
/* BR */ SET(SPI_BR_SPPR(0))|SET(SPI_BR_SPR(2)), \
/* ML */ 0, \
/* MH */ 0, \
}
SPI0_Init( SPI_MODULE_CUSTOM_CONFIG, NULL, 0, NULL);
DMA_InstallCallbackDMA0( PRI_LVL3, &dma_cb );
DMA0_Init(DMA_CH_SWTRG_M2P_CN_CONFIG(data,DMA_SIZE8BIT,0x40075006,4));
while(DMA_IsDone(DMA0));
// Callback for DMA
void dma_cb(DMA_CH_CALLBACK_TYPE type)
{
if( type == DONE_CALLBACK )
{
}
}