Hello,
i have a mk22fx512 and i use KDS 3.2 with SDK1.3. I have a SDHC card connected to the SDHC interface that i will use with the msd class. The problem is that the firmware read the USB_MSC_DEVICE_GET_INFO but windows get usb device not recognized.
I have attach the firmware. Can you help me?
Thanks
Original Attachment has been moved to: Test.zip
HI Daniele Cortellazzi
I saw that you have a USB PE project, I recommend you to better use our last usb stack that is with SDK_2.x.
About your issue, could you please refer to the following links and document:
Creating a New USB project with KSDK and Processor Expert support in KDS
USB Host Project with KSDK 1.3 and Processor Expert
USB for the TWR-K21F120M | MCU on Eclipse
These posts explain how to create a project with PE support; the second one refer to a host project, but it could give you some guides, for example, it tells about "Memory Allocation Considerations" in chapter 9 (when working with PE and USB you need to change some configurations that comes with PE by default).
Hope this information could help you.
Have a great day,
Jorge Alcala
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------