No wsd project files in the demo folder of sdk 2.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No wsd project files in the demo folder of sdk 2.1

1,174 次查看
roymessinger
Contributor V

Hi,

I'm a newbie in the FRDM K64 board (and in ARM in particular). I've downloaded the KDS software and the SDK 2.1 file, unzipped it, followed all the instructions to load a Hello World project, but... no wsd project files are available in the demo folder.

All the tutorials I've found in NXP website points to that demo folder. What is going on?

I've downloaded IAR sdk, and in the demo folder of that zip file, they do have all the projects files of IAR, but I want to work with KDS...

Only files I have in that folder of KDS are: setting folder and .cproject & .project files. that's it.

Thanks.

标签 (1)
1 回复

997 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use IAR, you just need to double click the *.eww, the example project will be imported into the IAR, you can make it, it is okay.

If you use KDS tools, you need follow up the procedures:

1)load KDS tools, click File->import, then in the IMPORT menu, select General->Existing Project into Workspace, then click next, browse the project you want to import, it is okay.

Hope it can help you

BR

Xiangjun rong