No 'flashx' drivers in KSDK with MQX for KDS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No 'flashx' drivers in KSDK with MQX for KDS?

ソリューションへジャンプ
1,288件の閲覧回数
M_Grillo
Contributor III

It’s safe to say that with the K64 and KSDK using MQX you can no longer use the original MQX “flashx” drivers and you have to use the KSDK flash methods in “FlashProgram.c” as shown in “flash_demo_twrk64f120m” ?

 

Thanks,

Mark

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
921件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mark:

Yes, that is true. With MQX for KSDK the classic MQX drivers are not used. Instead you have the KSDK platform drivers. In this case the Flash driver is in the path "C:\Freescale\KSDK_1.1.0\platform\drivers\src\flash" and it is the same as the C90TFS Standard Software Driver.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
922件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mark:

Yes, that is true. With MQX for KSDK the classic MQX drivers are not used. Instead you have the KSDK platform drivers. In this case the Flash driver is in the path "C:\Freescale\KSDK_1.1.0\platform\drivers\src\flash" and it is the same as the C90TFS Standard Software Driver.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
921件の閲覧回数
M_Grillo
Contributor III

Thanks Jorge for the clarification!

Mark

0 件の賞賛
返信