大家好,我在用KINETIS-SDK包
和KL26芯片
开发UART0收送功能时,老报错,是不是SDK不支持KL26的UART0?
代码大致如下,还是我哪里设置的不对?
| uint8_t buf[17] = {0xAA,0x55}; | |
| uart_user_config_t uartConfig; | |
| uartConfig.baudRate = 9600; | |
| uartConfig.bitCountPerChar = kUart8BitsPerChar; | |
| uartConfig.parityMode = kUartParityDisabled; | |
| uartConfig.stopBitCount = kUartOneStopBit; | |
| uart_state_t uartState; |
| hardware_init(); |
| SIM_SOPT2 |= SIM_SOPT2_PLLFLLSEL_MASK; | |
| SIM_SOPT2 |= SIM_SOPT2_UART0SRC(1); | |
| SIM_SCGC4 |= SIM_SCGC4_UART0_MASK; |
| PORTE_PCR20 |= PORT_PCR_MUX(0x4); | ||
| PORTE_PCR21 |= PORT_PCR_MUX(0x4); |
| UART_DRV_Init(0, &uartState, &uartConfig); | |
| while(1) | |
| { | |
| UART_DRV_SendData(1,buf,17); | |
| ;//断点 | |
| } |
Hi Shihao,
在回答你问题之前,我想知道一下你的SDK的版本是多少?
还有你说的收发错误,我知道具体表现是什么样子的呢?
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Shihao,
在KSDK1.2中,关于KL26的hello_world工程,本身就在hardware_init();中已经初始化了UART0,所以肯定KL26是支持UART0的。
我建议你可以先在main()中,先禁止使能你自己对UART0的配置,在debug中看看经过hardware_init();后,UART0的寄存器值。
并在下次过程中,禁止hardware_init();中关于对UART0配置的部分,然后使用自己的代码,在debug中看看使用你自己的代码配置后,UART0的寄存器值,
然后比较一下前后两次的差别。
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------