Hello,
I'm running into a intriguing problem.
Some time ago, I could successfully help a customer, by creating an example code with Processor Expert based on KSDK MQX USB Host - FATfs demo for K64. The KSDK version was 1.2.0 yet. Now, another customer needed the same example code for MK22FN1M0. I carefully followed the same steps with KSDK 1.3.0, but it didn't work this time. I got "Error 1" build error. I have no idea what caused this error and I have spent a lot of time trying to find it out.
Probably I missed something.
Can anybody help me please?
My project is attached.
Thanks and best regards,
Marco Coelho
Applicattions Engineer
Siletec Eletronica
Original Attachment has been moved to: teste_msd_k22.zip
解決済! 解決策の投稿を見る。
Hello Marco,
I tried by using the plug-in version 2.4 instead of the new one. It compiled successfully.
Could you please try by using this version?
I hope this can help.
Best Regards,
Isaac
Hello again,
I just tried to create a new Processor Expert project with a FRDM-K64F that I have here, based on demo again. But I got the same Error 1 that explains absolutely nothing! This time, I didn't use fsl_usb_framework bean. I added all SDK files and their paths manually.
We are really stuck on that now and we need urgent solution for that more than ever! Can anybody give us a helping hand?
Thanks and best regards,
Marco Coelho
Hello Marco,
I compiled your project and see that linker is failing due wrong names on .o files.
Please see this post Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse.
After installing the make.exe and echo.exe in KDS files, project compiles correctly.
I hope this can help you.
Have a nice day!
Best Regards,
Isaac
----------------------------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------------------------
Even for new projects (no matter which workpace they are at), the *.elf file is not generated anymore after the (make.exe, rm.exe and echo.exe and inclusion of sh.exe and busybox.exe) files replacement.
Hello Marco,
I tried by using the plug-in version 2.4 instead of the new one. It compiled successfully.
Could you please try by using this version?
I hope this can help.
Best Regards,
Isaac
Isaac,
I just found version 2.4 and I will make a new test.
Hello, Isaac
The problem was the version 2.6. I installed version 2.4 and replaced the files in KDS/bin folder and everything is working fine now!
I would never find it out by myself.
I'm very grateful for your great support, guys!
Best regards!
Marco Coelho
Applications Engineer
Siletec Eletronica
Hi Marco,
I used your attached project to build (update 2.4 plug in), and I got the following error. Can you get the similar error? I have search "update_state" in the project, there is only found in os_tasks.c, that means there is not define in the project.
C:\Users\shen\Documents\myspace\teste_msd_k22\Debug/../Sources/os_tasks.c:143: undefined reference to `update_state'
makefile:96: recipe for target 'teste_msd_k22.elf' failed
collect2.exe: error: ld returned 1 exit status
make: *** [teste_msd_k22.elf] Error 1
Hello Zhong,
I think that I commented this calling in order to compile the project correctly.
Could you validate this?
Best Regards,
Isaac
Hello Isaac,
Yes, thanks.
Best regard,
Zhong Shen
Hi, Isaac
Where can I find this plug-in?
With the new make.exe/etc, what is the command line (console view) saying?
Maybe there is a permission problem with the new make.exe/etc.: can you try to call them from the cmd.exe (DOS shell) if you can launch them?
Otherwise it could be that your firewall/virus scanner is intercepting the calls to the commands?
Erich
Hello, Erich
As I told previously to Isaac, my Console View after inserting the new files, is:
09:54:19 **** Build of configuration Debug for project teste_msd_k22 ****
make all
09:54:19 Build Finished (took 94ms)
And the elf file is not generated after compiling any project in KDS anymore.
When I executed make.exe in cdm.exe (DOS shell), I got the following:
The dialogue box brings up a message in portuguese that says it is missing a file called intl.dll in my computer and it recommends to reinstall it. Where do I find this file to reinstall?
Executing rm.exe, echo.exe and busybox, I have:
"sh.exe" just prints out the money sign "$":
I tried to disable my Anti-Virus, but the error remains.
Thank you!
Hello, Isaac
I returned the old rm.exe, make.exe and echo.exe to bin folder, cleaned and rebuilt the project to see what is the console. Take a look at that:
16:56:25 **** Incremental Build of configuration Debug for project teste_msd_k22 ****
make all
'Building target: teste_msd_k22.elf'
'Invoking: Cross ARM C++ Linker'
arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -Wall -g3 -T "C:/Users/Marco-Siletec/workspace2.kds/teste_msd_k22/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"C:/Users/Marco-Siletec/workspace2.kds/teste_msd_k22/Project_Settings/Linker_Files" -Wl,-Map,"teste_msd_k22.map" -lgcc -lc -lsupc++ -lm -specs=nosys.specs -nostartfiles -Xlinker -z -Xlinker muldefs -Xlinker -static -o "teste_msd_k22.elf" ./Static_Code/System/PE_low_level_init.o ./Static_Code/System/Peripherals_Init.o ./Static_Code/Peripherals/FMC_Init.o ./Sources/fatfs/option/unicode.o ./Sources/fatfs/diskio.o ./Sources/fatfs/ff.o ./Sources/Events.o ./Sources/main.o ./Sources/msd_diskio.o ./Sources/msd_fat_demo.o ./Sources/os_tasks.o ./Sources/rtos_main_task.o ./SDK/usb/usb_core/host/sources/controller/khci/host_khci_interface.o ./SDK/usb/usb_core/host/sources/controller/khci/khci.o ./SDK/usb/usb_core/host/sources/controller/ehci/ehci_host.o ./SDK/usb/usb_core/host/sources/controller/ehci/host_ehci_interface.o ./SDK/usb/usb_core/host/sources/controller/usb_host.o ./SDK/usb/usb_core/host/sources/controller/usb_host_ch9.o ./SDK/usb/usb_core/host/sources/controller/usb_host_common.o ./SDK/usb/usb_core/host/sources/controller/usb_host_dev_mng.o ./SDK/usb/adapter/sources/sdk/adapter_sdk.o ./SDK/rtos/mqx/mqx_stdlib/source/strings/strings.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/buf_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/err.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fclose.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fflush.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fopen.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fp_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fread.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/fwrite.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/get.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/pos.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/print.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/print_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/put.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/scan.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/scan_prv.o ./SDK/rtos/mqx/mqx_stdlib/source/stdio/stdio.o ./SDK/rtos/mqx/mqx/source/string/str_utos.o ./SDK/rtos/mqx/mqx/source/string/strnlen.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/core/M4/boot.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/core/M4/dispatch.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/core/M4/support.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/compiler/gcc_arm/comp.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/cortex.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_gkis.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_kisr.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_pvta.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_unx.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_vtab.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/int_xcpt.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/ipsum.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/mem_copy.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/mem_zero.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/nvic.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_dati.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_gelms.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_hoti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_iinit.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mat1.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mat2.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mat3.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_miti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_msti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_mstiq.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_nsti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_psti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_seti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_supp.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tiad.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tida.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tihr.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_timn.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tims.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tinm.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tins.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tiol.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tipr.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tips.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tise.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tisu.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tius.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_tkti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/psp_usti.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/sc_irdyq.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/stack_bu.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/stack_de.o ./SDK/rtos/mqx/mqx/source/psp/cortex_m/stack_st.o ./SDK/rtos/mqx/mqx/source/nio/src/errno.o ./SDK/rtos/mqx/mqx/source/nio/src/nio.o ./SDK/rtos/mqx/mqx/source/nio/src/nio_posix.o ./SDK/rtos/mqx/mqx/source/nio/src/nio_std_adpt.o ./SDK/rtos/mqx/mqx/source/nio/fs/fs_supp.o ./SDK/rtos/mqx/mqx/source/nio/drivers/nio_tty/src/nio_tty.o ./SDK/rtos/mqx/mqx/source/nio/drivers/nio_serial/src/nio_serial.o ./SDK/rtos/mqx/mqx/source/nio/drivers/nio_dummy/src/nio_dummy.o ./SDK/rtos/mqx/mqx/source/kernel/event.o ./SDK/rtos/mqx/mqx/source/kernel/idletask.o ./SDK/rtos/mqx/mqx/source/kernel/inittask.o ./SDK/rtos/mqx/mqx/source/kernel/int.o ./SDK/rtos/mqx/mqx/source/kernel/klog.o ./SDK/rtos/mqx/mqx/source/kernel/log.o ./SDK/rtos/mqx/mqx/source/kernel/lwevent.o ./SDK/rtos/mqx/mqx/source/kernel/lwlog.o ./SDK/rtos/mqx/mqx/source/kernel/lwmem.o ./SDK/rtos/mqx/mqx/source/kernel/lwmsgq.o ./SDK/rtos/mqx/mqx/source/kernel/lwsem.o ./SDK/rtos/mqx/mqx/source/kernel/lwtimer.o ./SDK/rtos/mqx/mqx/source/kernel/mem.o ./SDK/rtos/mqx/mqx/source/kernel/mqx.o ./SDK/rtos/mqx/mqx/source/kernel/msg.o ./SDK/rtos/mqx/mqx/source/kernel/msgpool.o ./SDK/rtos/mqx/mqx/source/kernel/msgq.o ./SDK/rtos/mqx/mqx/source/kernel/mutex.o ./SDK/rtos/mqx/mqx/source/kernel/name.o ./SDK/rtos/mqx/mqx/source/kernel/partition.o ./SDK/rtos/mqx/mqx/source/kernel/queue.o ./SDK/rtos/mqx/mqx/source/kernel/sched.o ./SDK/rtos/mqx/mqx/source/kernel/sem.o ./SDK/rtos/mqx/mqx/source/kernel/task.o ./SDK/rtos/mqx/mqx/source/kernel/taskq.o ./SDK/rtos/mqx/mqx/source/kernel/time.o ./SDK/rtos/mqx/mqx/source/kernel/timer.o ./SDK/rtos/mqx/mqx/source/kernel/tlsf.o ./SDK/rtos/mqx/mqx/source/kernel/tlsf_adaptation.o ./SDK/rtos/mqx/mqx/source/kernel/watchdog.o ./SDK/rtos/mqx/mqx/source/bsp/init_bsp.o ./SDK/platform/utilities/src/fsl_debug_console.o ./SDK/platform/utilities/src/fsl_misc_utilities.o ./SDK/platform/utilities/src/print_scan.o ./SDK/platform/system/src/interrupt/fsl_interrupt_manager.o ./SDK/platform/system/src/hwtimer/fsl_hwtimer.o ./SDK/platform/system/src/hwtimer/fsl_hwtimer_systick.o ./SDK/platform/system/src/clock/MK22FA12/fsl_clock_MK22FA12.o ./SDK/platform/system/src/clock/fsl_clock_manager.o ./SDK/platform/system/src/clock/fsl_clock_manager_common.o ./SDK/platform/osa/src/fsl_os_abstraction_mqx.o ./SDK/platform/hal/src/uart/fsl_uart_hal.o ./SDK/platform/hal/src/sim/MK22FA12/fsl_sim_hal_MK22FA12.o ./SDK/platform/hal/src/rtc/fsl_rtc_hal.o ./SDK/platform/hal/src/port/fsl_port_hal.o ./SDK/platform/hal/src/osc/fsl_osc_hal.o ./SDK/platform/hal/src/mpu/fsl_mpu_hal.o ./SDK/platform/hal/src/mcg/fsl_mcg_hal.o ./SDK/platform/hal/src/mcg/fsl_mcg_hal_modes.o ./SDK/platform/drivers/src/uart/fsl_uart_common.o ./SDK/platform/drivers/src/uart/fsl_uart_driver.o ./SDK/platform/drivers/src/rtc/fsl_rtc_common.o ./SDK/platform/drivers/src/mpu/fsl_mpu_common.o ./SDK/platform/drivers/src/mpu/fsl_mpu_driver.o ./SDK/platform/devices/MK22FA12/startup/gcc/startup_MK22FA12.o ./SDK/platform/devices/MK22FA12/startup/system_MK22FA12.o ./SDK/platform/devices/startup.o ./Generated_Code/SDK/usb/usb_core/host/sources/bsp/usbFmw1_host_bsp.o ./Generated_Code/SDK/usb/usb_core/host/sources/bsp/usb_host_bsp.o ./Generated_Code/Cpu.o ./Generated_Code/MainTask.o ./Generated_Code/clockMan1.o ./Generated_Code/flash_drive.o ./Generated_Code/fsl_hwtimer1.o ./Generated_Code/fsl_mpu1.o ./Generated_Code/hardware_init.o ./Generated_Code/mqx_ksdk.o ./Generated_Code/osa1.o ./Generated_Code/pin_mux.o ./Generated_Code/uart1.o ./Generated_Code/usbFmw1.o C:/Freescale/KSDK_1.3.0/usb/usb_core/host/lib/mqx/kds/MK22F51212/debug/libusbh_mqx.a C:/Freescale/KSDK_1.3.0/lib/ksdk_mqx_lib/kds/K22F51212/debug/libksdk_platform_mqx.a C:/Freescale/KSDK_1.3.0/rtos/mqx/lib/frdmk22f.kds/debug/mqx/lib_mqx.a C:/Freescale/KSDK_1.3.0/rtos/mqx/lib/frdmk22f.kds/debug/mqx_stdlib/lib_mqx_stdlib.a
arm-none-eabi-g++: error: C:/Freesale/KSDK_1.3.0/usb/usb_core/host/lib/mqx/kds/MK22F51212/debug/libusbh_mqx.a: No such file or directory
make: *** [teste_msd_k22.elf] Error 1
16:56:27 Build Finished (took 1s.718ms)
Notice that the error refers to a wrong name in USB Host MQX library file path. Instead of c:/Freescale..., it is looking for "C:/Freesale...". That is driving me crazy! How can I fix that?
Marco Coelho
Your problem is that you execeed the 8192 character limit on Windows.
You need to apply the following patch described here:
Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse
Windows will cut out some characters from your command line, resulting in these strange errors.
Erich
And now I can't generate .elf file for all other projects in the same workspace.
Hello, Isaac
After performing the changes you recommended, the Error 1 disappeared, but it looks like the compiler is not building the project anymore. The *.elf file is not generated and I don't see anything in Console after cleaning and building the project: