Link to SDK v1.3 KDS plug-in update for PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Link to SDK v1.3 KDS plug-in update for PE

1,462 Views
Cdn_aye
Senior Contributor I

I need to use the PE components and need a way to use KDS with the sdk v1.3, which I think was the last version supported for PE. I can't find any links for the plug-in or the sdk v1.3. It looks like the links have been scrubbedd. A png file on the NXP site pops up on which just says "DOWNLOAD". I think it was a fast way to kill the download without changing the web contents.

Can anyone share the links or plug-ins for the above? Thanks

Robert

Labels (1)
Tags (4)
0 Kudos
Reply
2 Replies

1,252 Views
Cdn_aye
Senior Contributor I

Hi Marek

Thank you for helping.

Regards

Robert

0 Kudos
Reply

1,252 Views
marek-trmac
NXP Employee
NXP Employee

Hi Robert,

  • go to nxp.com/ksdk
  • select DOWNLOADS in top menu bar
  • scroll down and select `Kinetis SDK`
  • continue with KSDK v1.3.0 Mainline releases

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button