Link to SDK v1.3 KDS plug-in update for PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Link to SDK v1.3 KDS plug-in update for PE

1,510件の閲覧回数
Cdn_aye
Senior Contributor I

I need to use the PE components and need a way to use KDS with the sdk v1.3, which I think was the last version supported for PE. I can't find any links for the plug-in or the sdk v1.3. It looks like the links have been scrubbedd. A png file on the NXP site pops up on which just says "DOWNLOAD". I think it was a fast way to kill the download without changing the web contents.

Can anyone share the links or plug-ins for the above? Thanks

Robert

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,300件の閲覧回数
Cdn_aye
Senior Contributor I

Hi Marek

Thank you for helping.

Regards

Robert

0 件の賞賛
返信

1,300件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Robert,

  • go to nxp.com/ksdk
  • select DOWNLOADS in top menu bar
  • scroll down and select `Kinetis SDK`
  • continue with KSDK v1.3.0 Mainline releases

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button