Kinetis SDK support for KEA automotive series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis SDK support for KEA automotive series

Jump to solution
3,432 Views
stl
Contributor I

KDS 3.0 supports KEA Series, but KSDK 1.2 does not. Is that correct?

If yes, when is it supposed to be supported?

Thanks a lot

HLE

Labels (1)
0 Kudos
Reply
1 Solution
2,599 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Helmut,

KDS V.3.0 supports KEA family, you are right

kea.png

but unfortunatelly - there is no KSDK support for Automotive - KEA series.

Currently we do not have any plan for the family.

If will be some changes I will let you know.

Have a nice day!

Best Regards,

Iva

View solution in original post

8 Replies
2,599 Views
nirmalakunwar
Contributor I

Hi,

What do you suggest to use as development  environment for KEA series.

0 Kudos
Reply
2,599 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Nirmala,

I suggest to you choose on of the option mentioned here

Kinetis KEA|ARM Cortex-M0+|32-bit Automotive MCUs|NXP

I hope this helps!

Best Regards,

Iva

0 Kudos
Reply
2,599 Views
nirmalakunwar
Contributor I

Thanks Iva. Do you suggest using KDS or S32 Design Studio for kEA128 developement.

0 Kudos
Reply
2,599 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Nirmala.

I suggest S32 Design Studio for Automotive MCUs.

We have a big space for answering questions regarding this IDE S32 Design Studio

The newest KDS v.3.2 is supposed to be used in combination with KSDK and KEA family is not supported by KSDK.

There is project wizard to create bare metal, Kinetis KDK v1.x and v2 and Processor Expert software projects.

Or you can use KDS 3.0 with PEx and use LDD components to initialize and configure their peripherals.

In case of any questions, please let me know.

Best Regards,

Iva

0 Kudos
Reply
2,600 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Helmut,

KDS V.3.0 supports KEA family, you are right

kea.png

but unfortunatelly - there is no KSDK support for Automotive - KEA series.

Currently we do not have any plan for the family.

If will be some changes I will let you know.

Have a nice day!

Best Regards,

Iva

2,599 Views
Novalis
Contributor III

Hello Iva,

still no news about KEA (or at least KE) support in KSDK?

I would like to replace Coldfire V1 MCF51JM  with Kinetis and KEA128 seems to be the best solution.

Thanks,

Martin

2,599 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Martin,

at the moment no, KEA is no currently on the roadmap.

Sorry for the inconvenience this may caused.

Best Regards,

Iva

0 Kudos
Reply
2,599 Views
mjbcswitzerland
Specialist V

Hi Helmut

The uTasker project supports KEA family in KDS:

µTasker TRK-KEA128 support

This includes KBOOT compatible loader and simulation of the device and boards.

Note however that the KEA devices are very similar to KE parts so you can in fact use a KE project and make just a few changes to work on the KEAs.

Regards

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support  / µTasker FRDM-KE02Z40M support  / µTasker FRDM-KE06Z support

KEA: µTasker TRK-KEA128 support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply