KSDK w/MQX True C++ support (i.e. <iostream> <string> etc.)?  Needed for CppUnit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK w/MQX True C++ support (i.e. <iostream> <string> etc.)?  Needed for CppUnit

1,143件の閲覧回数
stevenneves
Contributor I

I'm using KSDK 1.2 with MQX (full).  I've used the previous CW MQX BSP's in the past but have migrated to KSDK with the goal of using C++.  The main reason behind this is the stitch in CppUnit (C++ based unit testing framework).  In the past I've had to link in my applications source and run in it via cygwin, completely bypassing MQX and guarding my code to ignore any OS level calls during my unit test build.  I want to be able to run my unit test build on hardware.  I've created test projects that had .cpp files in it with a relatively simple class and a few public functions.  Everything seemed fine until I decided to use <iostream> and <string>.  Basically stdio.h (MQX's implementation) re-declares FILE which the C++ compiler does not appreciate very much.  After much struggling I was actually able to get CppUnit to compile but it doesn't properly launch and is stuck in a reset loop at line 69 of boot.S.  Does anyone have any experience implementing a unit test framework into KSDK with MQX, and what exactly is the extent of C++ support if using MQX.  Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

912件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Steven,

this is what I achieved on using C++ with MQX for KSDK.

How to Create a C++ Project Using MQX RTOS for KSDK1.2

If you have a specific use case that does not work would you share a simple code please?

Regards,

Carlos

0 件の賞賛
返信