KSDK 2.0 usb_host_config.h for KL26Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK 2.0 usb_host_config.h for KL26Z

Jump to solution
793 Views
enchanter
Contributor I

I would like to use the USB host on a KL27Z to write a USB flash drive. I downloaded the KSDK 2.0 for the FRDM-KL27Z board and IAR running on Windows. In the second step in the USB Stack User's Guide (section 4.2.2.1), the file usb_host_config.h is copied to an application directory; however, there is no usb_host_config.h file in the KDSK. All of the KDSK examples are for the USB device. Where is usb_host_config.h for the KL27Z?

Labels (1)
Tags (1)
1 Solution
565 Views
DavidS
NXP Employee
NXP Employee

Hi Tim,

The KL27 is USB device only (crystal-less USB).

The KL26 and KL46 (USB OTG Host and Device support) will have KSDK_v2 support end of March per Introducing Kinetis SDK v2 .

Regards,

David

View solution in original post

1 Reply
566 Views
DavidS
NXP Employee
NXP Employee

Hi Tim,

The KL27 is USB device only (crystal-less USB).

The KL26 and KL46 (USB OTG Host and Device support) will have KSDK_v2 support end of March per Introducing Kinetis SDK v2 .

Regards,

David