Hello ,
Yes , it have not support this chip so far , you can use the Processor Expert development
your project now , this bin also convenient to develop .
About the PE, there are demo code about the component in the "help on component",
for example the ADC component :
You can refer to the demo code to use the functions .
Hope it helps
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Alice Yang
The MK22FN1M0 is supported with FreeRTOS. It is available from the McuOnEclipse project:
The latest FreeRTOS port for it is available on SourceForge (SourceForge.net ), see Releases on SourceForge how to install it.
As a bonus, you can use it with the Percepio Trace (FreeRTOS Continuous Trace Streaming) or with the Segger System Viewer (Segger SystemView: Realtime Analysis and Visualization for FreeRTOS).
I hope this helps,
Erich