KSDK 1.3.0 support for  MK22FN1M0xxx12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK 1.3.0 support for  MK22FN1M0xxx12

1,378件の閲覧回数
daafies
Contributor II

Hi, i am unable to create a project for MK22FN1M0xxx12 with KSDK 1.3.0

 

am i missing an update? when will it be supported? thanks

david

 

118838_118838.pngpastedImage_1.png

ラベル(1)
4 返答(返信)

1,274件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Yes , it have not support this chip so far , you can use the Processor Expert development

your project now , this bin also convenient to develop .

About the PE, there are demo code about the component in the "help on component",

for example the ADC component :

pastedImage_1.png

pastedImage_0.png

You can refer to the demo code to use the functions .

Hope it helps



-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,
Alice Yang

0 件の賞賛
返信

1,274件の閲覧回数
daafies
Contributor II

Thanks. I guess that means there is also no freertos and/or mqx port for it?

0 件の賞賛
返信

1,274件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The MK22FN1M0 is supported with FreeRTOS. It is available from the McuOnEclipse project:

pastedImage_0.png

The latest FreeRTOS port for it is available on SourceForge (SourceForge.net ), see Releases on SourceForge  how to install it.

As a bonus, you can use it with the Percepio Trace (FreeRTOS Continuous Trace Streaming) or with the Segger System Viewer (Segger SystemView: Realtime Analysis and Visualization for FreeRTOS​).

I hope this helps,

Erich

1,274件の閲覧回数
daafies
Contributor II

thanks !

0 件の賞賛
返信