KDS 3.0 and KSDK 1.3.0 frdmk22f - cannot get UAR working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS 3.0 and KSDK 1.3.0 frdmk22f - cannot get UAR working

909 Views
aroste
Contributor IV

Hi all, 

I have a board based on this development board,  In the project I have mqx, board and hardware init file specific to my hardware.  

 

I use several I/O and 2 SPI that work fine. (it seems)

 

I want to implement an UART but without success. I tried the different solutions from the examples but no way.  

 

I have a specific task just for the UART, in init I call 

UART_DRV_Init(UART2, &uartState, &uartConfig);

 

I tried to add install RxCallback, etc..  

 

I miss something ?

 

Thanks

BR

 

P.S: The BSP debug UART1 init code is commented.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

816 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I am sorry for the delay.

Do you use the board FRDM-K22F or your own board based on the FRDM-K22F?

For uart test, I suggest you output the char and hook a scope to the UART2_TX to check if there is signal.

If you do not have signal, pls check the pin assignment.

BR

Xiangjun Rong

0 Kudos
Reply