I have installed KDS 2.0 with KSDK 1.0 as per AMF-SDS-D0805 (page 101) to summarize i did the following steps
Installed KDS 2.0
Installed MQX_KSDK_1.0.0
Apply update in Eclipse for MQX_KSDK
File->New->Kinetis Design Studio project
Enter Project Name, location, NEXT
Select FRDM-K64F under Boards->Kinetis, NEXT
Select Kinetis SDK and Processor Expert (to get MQX_SDK - RTOS and MQX_SDK_Task to create main)
Once it loads everything I have 6 warnings dealing with PIN Muxing conflicts (below)
Am I doing something wrong? Normally when our tools have direct support for a specific target it just works with no errors...
Yes these aren't *errors* but still it is not a 'clean' build.
| Description | Resource | Path | Location | Type |
| Ignored error: Selected value is in conflict with other configuration(s) property 'Pin 6', property 'P10 - Wake-up pin 10', property 'Pin' from component gpio_pins Exclusive connection required by ; Selected value is in conflict with other configuration property 'Pin' from component gpio_pins, property 'Pin 6', conflict in configuration of MUX bit-field of PORTC_PCR6 register. (MCLK - Master clock) | test5 | | pin_mux/MCLK - Master clock | Processor Expert Problem |
| Ignored error: Selected value is in conflict with other configuration property 'TX - transmitter output', conflict in configuration of MUX bit-field of PORTB_PCR18 register. ; Selected value is in conflict with other configuration(s) property 'TX - transmitter output' Exclusive connection required by property 'TX - transmitter output' (TX_BCLK - TX bit clock) | test5 | | pin_mux/TX_BCLK - TX bit clock | Processor Expert Problem |
| Ignored error: Selected value is in conflict with other configuration(s) property 'Pin 6', property 'Pin' from component gpio_pins Exclusive connection required by property 'Pin 6' or property 'Pin' from component gpio_pins; Selected value is in conflict with other configuration property 'Pin 6', property 'Pin' from component gpio_pins, conflict in configuration of MUX bit-field of PORTE_PCR6 register. (CH1 - Channel 1) | test5 | | pin_mux/CH1 - Channel 1 | Processor Expert Problem |
| Ignored error: Selected value is in conflict with other configuration(s) property 'Pin' from component gpio_pins, property 'Pin 8' Exclusive connection required by property 'Pin' from component gpio_pins or property 'Pin 8'; Selected value is in conflict with other configuration property 'Pin 8', property 'Pin' from component gpio_pins, conflict in configuration of MUX bit-field of PORTE_PCR8 register. (TX - Transmit data) | test5 | | pin_mux/TX - Transmit data | Processor Expert Problem |
| Ignored error: Selected value is in conflict with other configuration(s) property 'Pin 9', property 'Pin' from component gpio_pins Exclusive connection required by property 'Pin 9' or property 'Pin' from component gpio_pins; Selected value is in conflict with other configuration property 'Pin 9', property 'Pin' from component gpio_pins, conflict in configuration of MUX bit-field of PORTE_PCR9 register. (RX - Receive data) | test5 | | pin_mux/RX - Receive data | Processor Expert Problem |
| Ignored error: Selected value is in conflict with other configuration(s) property 'RX - receiver input' Exclusive connection required by property 'RX - receiver input'; Selected value is in conflict with other configuration property 'RX - receiver input', conflict in configuration of MUX bit-field of PORTB_PCR19 register. (TX_FS - TX frame sync) | test5 | | pin_mux/TX_FS - TX frame sync | Processor Expert Problem |