K64F USB CDC in KSDK 1.3.0 and PEx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64F USB CDC in KSDK 1.3.0 and PEx

ソリューションへジャンプ
1,470件の閲覧回数
bjorn_almqvist
Contributor I

Hi everyone!

 

I'm trying to get the usb cdc class example get up and running on a FRDM-K64F board when configuring my MK64F processor in processor expert. I've tried to follow some previous thread here but without any luck. It's always ends the same way, the examples are running just fine but when I try to create a new project with processor expert and port the code it's not recognized as a COM port. I get the error "USB device not recognized".

 

I need to use the KSDK 1.3.0, but the examples I've seen is using KSDK 1.2.0, so what am I missing to get it working?

 

I would really appreciate some help to get my project going. I attached my code and once it is working I will share it on this forum because I'm not the first one to ask questions about this.

 

 

Thank you all!

Original Attachment has been moved to: usb_cdc_virtual_com_mk64f12.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,253件の閲覧回数
PitOn
Contributor III
0 件の賞賛
返信
2 返答(返信)
1,253件の閲覧回数
bjorn_almqvist
Contributor I

Thank you very much! :smileyhappy:

The thing I didn't do was to set the correct stack and heap size.

With Best Regards,

/ Bjoern

0 件の賞賛
返信
1,254件の閲覧回数
PitOn
Contributor III
0 件の賞賛
返信