K64F USB CDC in KSDK 1.3.0 and PEx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64F USB CDC in KSDK 1.3.0 and PEx

Jump to solution
1,475 Views
bjorn_almqvist
Contributor I

Hi everyone!

 

I'm trying to get the usb cdc class example get up and running on a FRDM-K64F board when configuring my MK64F processor in processor expert. I've tried to follow some previous thread here but without any luck. It's always ends the same way, the examples are running just fine but when I try to create a new project with processor expert and port the code it's not recognized as a COM port. I get the error "USB device not recognized".

 

I need to use the KSDK 1.3.0, but the examples I've seen is using KSDK 1.2.0, so what am I missing to get it working?

 

I would really appreciate some help to get my project going. I attached my code and once it is working I will share it on this forum because I'm not the first one to ask questions about this.

 

 

Thank you all!

Original Attachment has been moved to: usb_cdc_virtual_com_mk64f12.zip

Labels (1)
0 Kudos
Reply
1 Solution
1,258 Views
PitOn
Contributor III
0 Kudos
Reply
2 Replies
1,258 Views
bjorn_almqvist
Contributor I

Thank you very much! :smileyhappy:

The thing I didn't do was to set the correct stack and heap size.

With Best Regards,

/ Bjoern

0 Kudos
Reply
1,259 Views
PitOn
Contributor III
0 Kudos
Reply